메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

TPS-1 PROFINET V2.3 Redundancy or MRP

Last Updated:06/02/2017

Question:

Can the TPS-1 stack support PROFINET V2.3 redundancy?

Answer:

PROFINET V2.3 redundancy is the same as Media Redundancy Protocol (MRP). Therefore, yes, TPS-1 supports PROFINET V2.3 redundancy, otherwise known as MRP.
Suitable Products
TPS-1
  • 이 기사가 도움이 되셨나요?