메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

TPS-1 SPI Clock for Flash Interface

Last Updated:06/01/2017

Question:

Can the customer change the clock of the SPI flash interface?

Answer:

The clock is set by the firmware and cannot be changed by the customer.
Suitable Products
TPS-1
  • 이 기사가 도움이 되셨나요?