메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

TPS-1 Support of Combined Fiber and Copper Ports

Last Updated:06/01/2017

Question:

Can TPS-1 support combined use of both a fiber port and a copper port?

Answer:

Yes, TPS-1 can support fiber and copper at same time.
Suitable Products
TPS-1
  • 이 기사가 도움이 되셨나요?