메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

TPS-1 USB and PCI Support

Last Updated:06/01/2017

Question:

Does the TPS-1 support USB or PCI interfaces?

Answer:

The TPS-1 does not have a USB or PCI interface. However, if such interfaces are required, they can be implemented via a host CPU.
Suitable Products
TPS-1
  • 이 기사가 도움이 되셨나요?