메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

TPS-1 Variable "L" in SPI Slave Interface

Last Updated:06/01/2017

Question:

What is the variable "L" in the TPS-1 user's manual in regards to the "SPI Slave Interface Handshake Wait"?

Answer:

"L" is the time between "end of of transfer" and subsequent "beginning of transfer".
Suitable Products
TPS-1
  • 이 기사가 도움이 되셨나요?