메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

UPD98410: Is there a way to set so that polling control is not performed?

Latest Updated:08/01/2005

Question:

For the UPD98410, is there a way to set so that polling control is not performed?

Answer:

No, there is not.
Polling is performed even in the single PHY mode.
Suitable Products
BD/DVD Recorder
Digital Camcorder
Industrial Network
  • 이 기사가 도움이 되셨나요?