메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

Are the Cob, fT etc. related with hFE as transistor characteristics?

Latest Updated:08/01/2005

Question:

Are the collector capacitance (Cob), transition frequency (fT), etc., correlated with the hFE rank as transistor characteristics?

Answer:

Generally, hFE and collector capacitance (Cob) are not correlated.
On the other hand, the transition frequency (fT) becomes lower if hFE declines because the current gain decreases as hFE decreases.
Suitable Products
Diodes for Constant Voltage