메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

Does on-resistance in forward direction constant in switching diode?

Latest Updated:11/01/2007

Question:

Is the on-resistance of the forward direction constant in a switching diode?

Answer:

No, the larger the forward current, the smaller the on-resistance. If the resistance were constant, the V-I characteristic would be a straight line, but in a diode, I increases exponentially as V increases. Since the resistance is V/I, the fact that the tangent (I/V) of the V-I characteristic curve forms a steep slope means that the resistance becomes lower.

Suitable Products
  • 이 기사가 도움이 되셨나요?