메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

How long are the on and off when using a transistor for amplification?

Latest Updated:11/01/2007

Question:

When using a transistor for amplification, about how long are the turn-on and turn-off times?

Answer:

An amplification transistor is not used for switching, so these times are not prescribed. If you need switching characteristics, please use a switching transistor.
Suitable Products
  • 이 기사가 도움이 되셨나요?