메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

What is Depletion?

Latest Updated:11/01/2005

Question:

Depletion

Answer:

This is a type of MOS FET. A depletion type MOS FET has a characteristic that the drain current flows when the gate voltage is 0 V.
Today, enhancement type MOS FETs are generally used.
Products are ranked by the current when the bias is zero.
Suitable Products
  • 이 기사가 도움이 되셨나요?