메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

What kind of diode should I use for D1 in SC of the 3-terminal regulator?

Latest Updated:09/01/2006

Question:

What kind of diode should I use for D1 in the Standard Circuit of the 3-terminal regulator's Connection section (assuming a connection whereby the OUTPUT pin has a higher voltage than the INPUT pin)?

Answer:

With the aim of mitigating damage to the power supply IC, we would recommend using a Schottky barrier diode. Note that the withstanding voltage of the diode must be equal to or higher than the voltage differential between INPUT and OUTPUT.
Suitable Products
CMOS Operational Amplifiers
Bipolar Operational Amplifiers
3 Terminal Regulators