메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

Why is safety standards needed to RE photocoupler and optical MOS FET?

Latest Updated:11/01/2007

Question:

Renesas Electronics' photocoupler and optical MOS FET products meet many overseas safety standards, but why is this necessary?

Answer:

There are regulations applying to the isolation of the primary circuit and secondary circuit in sets incorporating photocouplers (power supplies, FA devices, etc.). The photocoupler accomplishes this isolation function. Therefore, if the photocouplers meet these regulations, the sets themselves may be exempted from the relevant qualification tests. This is why Renesas Electronics has developed photocouplers to meet these overseas safety regulations.

The status of each of Renesas Electronics' photocoupler and optical MOS FET product in terms of meeting overseas safety regulations can be checked at the following URLs.
[Photocouplers]
optoelectronics/photocoupler/safety-p1  optoelectronics/photocoupler/safety-p2
[Optical MOS FETs]
/products/opto/ocmos/child/safetyocmos.jsp
Suitable Products
Blue-Violet Laser
Optical Sensors
Optical Storage Devices
Fiberoptic Devices
Photocouplers / Optocouplers
Solid State Relays (OCMOS FETs)
  • 이 기사가 도움이 되셨나요?