메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

Do you have other products which temperature coefficient is assured?

Latest Updated:02/01/2008

Question:

I heard that the 1SZ series voltage reference diodes with a guaranteed temperature coefficient will soon be discontinued. Are substitute products available for which temperature coefficients are guaranteed?

Answer:

No other Zener diodes for which temperature coefficients are guaranteed are available, but the high-precision variable shunt regulator uPC1093 is recommended.
Suitable Products
 
  • 이 기사가 도움이 되셨나요?