메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

How do product differ in series regulator if it has letter in the middle?

Latest Updated:03/01/2006

Question:

The part name of some series regulators have a letter in the middle, such as "uPC78L05". How do these products differ?

Answer:

This letter indicates the approximate output current characteristics of the series regulator (click here for details).

L: 0.1 A
N: 0.3 A
M: 0.5 A
(No symbol): 1.0 A

Suitable Products
Power Management Linear