메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

What is supply variation rejection (SVR) of an operational amplifier?

Latest Updated:12/01/2011

Question:

What is supply variation rejection (SVR) of an operational amplifier?

Answer:

SVR is the ratio of the power supply voltage to the varied input offset voltage when the input offset voltage has changed due to a change in the power supply voltage.
SVR expresses the extent to which power supply ripple or noise can be suppressed in the device.

SVR=Δ(V+-V-)/ΔVIO

Example) SVR in the uPC801 is 76 dB (typ). From this it can be calculated that when the SVR is 6.3 × 103 and the power supply voltage varies temporarily by 0.5 V due to external disturbance, VIO varies by 79 μV.

Suitable Products
Operational Amplifiers
USB2.0 Host/Peripheral Controller
M66596, R8A66597
UPD720150