메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

What's the difference between the standby and off current of uPC1099?

Latest Updated:12/01/2011

Question:

What is the difference between the "standby current" and "off current" of the uPC1099.

Answer:

Standby current : The output is shut down if the supply voltage drops below 8 V. The supply current in this state is called the standby current.
Off current : The supply current when the uPC1099 is turned off by using the ON/OFF pin while it operates normally is called the off current.
Suitable Products
Power Management Linear