메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

Why do output cuts off if I short circuited one output of uPC1100?

Latest Updated:11/01/2005

Question:

If I short-circuit one output in the uPC1100, only that output is cut off (both outputs are not cut off).

Answer:

The timer latch circuit may be malfunctioning. Check the items listed in A1 above.
Suitable Products
Power Management Linear