메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

What are the characteristics at 5 V of the uPC1251?

Latest Updated:12/01/2011

Question:

The Vo vs. Io (sink) characteristics of the uPC1251 at 15 V are shown. What are the characteristics at 5 V?

Answer:

The current drops slightly at 5 V but there are no major changes.
Refer to the characteristics at 15 V shown in the Data Sheet (Japanese).
Suitable Products
Operational Amplifiers
USB2.0 Host/Peripheral Controller
UPD720150