메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

Is there a rating for voltage supplied in anode and cathode from PS2561D?

Last Updated: 11/06/2017

Question:

There is an absolute maximum rating of the forward current (IF) on the light-emitting side of the PS2561D photocoupler, but is there also rating regarding the voltage supplied between the anode and the cathode?

Answer:

The voltage supplied between the anode and the cathode of the light-emitting element is limited by the power dissipation on the light-emitting side (forward current × forward voltage).

Suitable Products
Photocouplers / Optocouplers