메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

Is there a fault if junction temperature doesn't pass full max rating?

Latest Updated:12/01/2011

Question:

Is there any problem as the junction temperature does not exceed the absolute maximum rating, even if the ambient operating temperature exceeds the absolute maximum rating?

Answer:

Yes. The reliability cannot be guaranteed.
The value of even one parameter of the absolute maximum ratings must not be exceeded.
Suitable Products
3 Terminal Regulators
  • 이 기사가 도움이 되셨나요?