메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

Can I change an H8/3437, H8/3337 & H8/3297 designs to an H8S/21xx?

Latest Updated:03/23/2009

Question:

Can I change an H8/3437, H8/3337 & H8/3297 designs to an H8S/21xx?

Answer:

"Yes. The H8S/21xx parts are designed to be pin compatible with the earlier H8/300 devices. The following table shows the connection between families.

H8S/3437 Series100pinH8S/2144 Series

H8S/3337 Series80pinH8S/2134 Series"

Suitable Products
H8S/2668
H8S/2655
H8S/2643
H8S/2633
H8S/2628
H8S/2615
H8S/2612
H8S/2437
H8S/2368
H8S/2398, 2357
H8S/2355
H8S/2350
H8S/2345
H8S/2282, 2280
H8S/2276
H8S/2258, 2239, 2238, 2237, 2227
H8S/2245
H8S/2215
H8S/2214
H8S/2199R
H8S/2194
H8S/2172
H8S/2168
H8S/2158
H8S/2140B
H8S/2114R
H8S/2111B
H8S/2110B
  • 이 기사가 도움이 되셨나요?