메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

On which medium you provide the purchased version of Flash Programmer?

Latest Updated:12/11/2013

Question:

On which medium do you provide the purchased product version of the Renesas Flash Programmer and what licenses are available?

Answer:

The medium and licenses are as described below.

Medium: CD-ROM

Product name (Orderable part number: including the number of licenses)

  • Product name for one license
    R0C00000FDW12R

  • Product names for multiple licenses have the following form.
    R0C00000FDW12R#X

    Where X indicates the number of licenses (any of L5, LA, LT, and LX, with the meanings listed below).
    L5:5 licenses
    LA:10 licenses
    LT:20 licenses
    LX:Individual licenses

Remarks
1. For one license, the actual product name (orderable part number) does not include “#X”.
2. One license allows one PC.

Suitable Products
Renesas Flash Programmer