메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

The Renesas Flash Programmer V2 and V3 at the same time?

Last Updated:04/19/2017

Question:

Can I use both the Renesas Flash Programmer V2 and V3 (the commercial edition) at the same time?

Answer:

Yes, you can use them concurrently.

If you have Renesas Flash Programmer V2 (the commercial edition), you can update it to V3 free of charge.
If you purchase the Renesas Flash Programmer V3 (commercial edition), you can use both of them.

See below for the details:
[For V2 purchasers] Upgrade from V2 to V3 of the Renesas Flash Programmer
[For V3 purchasers] Settings for using V2 of the Renesas Flash Programmer after purchasing V3
 

Suitable Products
Renesas Flash Programmer
  • 이 기사가 도움이 되셨나요?