메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

How to establish set up an environment for simulator & HEW3 emulator?

Latest Updated:09/10/2007

Question:

[High-performance Embedded Workshop V.3]  I am going to use a compiler, a simulator and an emulator on High-performance Embedded Workshop3 together. But I cannot establish an development environment for them.

Answer:

Most of all problams in establishment of development environment with High-performance Embedded Workshop V.3.01.04 and the earlier have been soloved in High-performance Embedded Workshop V.3.01.04 and above. Please install one. Also see High-performance Embedded Workshop Download site for details.
Suitable Products
High-performance Embedded Workshop