메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

How to get proper display in watch window?

Latest Updated:10/05/2012

Question:

I can’t get the watch window, local window or stack trace window to display. In addition, I can no longer select watch, instant watch, local or stack trace from the menu. How can I get the proper display?

Answer:

To enable the watch window display and the selections for watch or instant watch from the menu, select [Debug Settings] in the [Debug] menu of the High-performance Embedded Workshop. In the debug settings dialog box (See Figure 1.), set the [Default debug format] in accordance with the compiler you are using (See Table 1.).
After setting, finish the High-performance Embedded Workshop, and reboot.

Table 1.

Compiler Default debug format
C/C++ Compiler Package for SuperH Family Elf/Dwarf2
C/C++ Compiler Package for H8SX, H8S, H8 Family
C Compiler Package for M16C Series [M3T-NC30WA] V.6 or later
C Compiler Package for R32C Series IEEE695_RENESAS
C Compiler Package for M32C Series [M3T-NC308WA]
C Compiler Package for M16C Series [M3T-NC30WA]
V.5.20 Release 1~V.5.45 Release 01
C Compiler Package for 740 Family [M3T-ICC740] IEEE695_ICC740



Figure 1.

Suitable Products
High-performance Embedded Workshop
E10A-USB
E8a
E10T-USB
E10A
E10T
E8
E7
E6000H
E6000
  • 이 기사가 도움이 되셨나요?