메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

How to perform the standard I/O on the HEW?

Latest Updated:09/10/2007

Question:

[High-performance Embedded Workshop V.4, V.3]  How can I perform the standard I/O on the High-performance Embedded Workshop?

Answer:

In order to create standard I/O, please check a check box for [Use I/O libraries] when building a project on High-performance Embedded Workshop. By enabling this option, it generates simulator specific low-level I/O routines. If you want to generate standard I/O to mutch your syste, you need to create the low-level I/O routines by yourself.
Please refer to 9.2 Creation of Initial Setting Programs in your C/C++ Compiler, Assembler, Optimizing Linkage Editor User’s Manual.
Suitable Products
High-performance Embedded Workshop