메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

How to select option build on the setting dialog box of HEW?

Latest Updated:09/10/2007

Question:

[High-performance Embedded Workshop V.4]  How can I select options of build on the setting dialog boxes of High-performance Embedded Workshop?

Answer:

See the upper right of the descriptions of build options in your manual. That shows how you get to dialog box to select the options.

For example, you activate […Standard Toochain] dialog box, and select a tab, then a category, and item. You can select options on dialog boxes you open.

When you want to use options which the manual does not say how to use, please open […Standard Toochain] dialog box by selecting […Standard Toochain] from [Build] in High-performance Embedded Workshop. Then select a compiler, an assembler and an optimizing linkage editor tabs. After selecting all of the tabs, select [Others] for category, and enter an option name in the user-specified option field.

Suitable Products
High-performance Embedded Workshop