메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

Is Default Options automatically add new file?

Latest Updated:09/10/2007

Question:

[High-performance Embedded Workshop V.4, V.3]  Is it possible to select default options automatically for a file newly added to a project?

Answer:

[In case of using High-performance Embedded Workshop4]

Yes, it is. Please select […Standard Toolchains] from [Build] in the High-performance Embedded Workshop menu. You can see files listed on the left side of the opening dialog box. Please open a folder of the file group you want to set the default settings to. Then, the [default options] icon is displayed in the folder. Click at the icon and click "OK" after options in the right side of the option dialog box are selected

This option is applied when a file of the file group is first added to the project.

[In case of using High-performance Embedded Workshop3]

Yes, it is. Only in case of a multiple build phase, the default option can be selected into a phase. Choose a phase from the [Options] menu. If a phase is a multiple build phase,a list is displayed on the left side of an option dialog box . Please open folder of file group which default option to be selected from the file list. The [default options] icon is displayed in the folder. Click at the icon and click OK after options in the right side of the option dialog box are selected.

This option is applied when a file of the file group is first added to the project.

Suitable Products
High-performance Embedded Workshop