메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

Migration from HEW to CS+_RX MCU

Last Updated:12/06/2017

Question:

I am planning to move tools for projects created by the High-performance Embedded Workshop (hereafter called HEW) (version 4.09.00.007) to CS+ according to the method of migration from HEW to CS+.

I want to see what is selected in the existing HEW project for the CPU part number displayed in the list of "MCU to use". However, I cannot find where the part number is recorded in the HEW.
How can I find it?
 

Answer:

When creating a project in HEW (version 4.09.00.007), you select the CPU series (e.g. RX600) and CPU type (e.g. RX62N). Therefore, the information of the CPU part name does not exist in a project in HEW.
Select the CPU part name you are using when starting migration of tools.
Suitable Products
RX Family
CS+
High-performance Embedded Workshop
  • 이 기사가 도움이 되셨나요?