메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

What to do if the expected result of standard CC-RX is not obtained?

Latest Updated:10/29/2014

Question:

I'm using the standard library functions for the CC-RX compiler, but I am not obtaining the results I expect. What might I be doing wrong ?

Answer:

In the source file, add a directive to include the header file of the standard library function you wish to use.

Example
If you wish to use the atof() function:
#include

If you still do not obtain the expected result, check that prototype declarations have been made for the functions you create.

Suitable Products
CS+ (formerly CubeSuite+)
High-performance Embedded Workshop
C/C++ Compiler Package for RX Family