메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

Where is Configure Proxy button on Configure Auto Update dialog box?

Latest Updated:12/04/2006

Question:

I can't use AutoUpdate because the "Configure Proxy" button on the "Configure AutoUpdate" dialog box isn't available.

Answer:

Please reconstruct the AutoUpdate environment with the following procedure.

  1. Uninstall the current version of AutoUpdate.
  2. Restart your computer.
  3. Download the AutoUpdate program from the download site.
  4. Install the downloaded AutoUpdate.
Suitable Products
High-performance Embedded Workshop
Auto Update Utility