메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

Can I use CC-RL compiler to link libraries or object files?

Latest Updated:04/24/2015

Question:

I am using the CC-RL compiler for RL78 devices. Can I use the CC-RL compiler to link libraries or object files created by using the CA78K0R compiler for the RL78 and 78K0R?

Answer:

You cannot use the CC-RL compiler to link such libraries or object files because they are in different formats. Please recreate them specifically for CC-RL.
Also note that the interface with functions differs in some respects between the CA78K0R and CC-RL compilers. You will need to check the interface if you are using the assembler or have defined assembly functions.
Suitable Products
e² studio
CS+ (formerly CubeSuite+)
C Compiler Package for RL78 Family