메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

Checking Free Space on ROM_CS+

Last Updated:12/20/2017

Question:

I am using the CS+ integrated development environment. Is there any method to check free space on ROM?

Answer:

ou can use a list file output by the linker to check the allocation of sections. In the list file, check the part to which no section has been allocated.

Note that CS+ for CC provides a memory mapping profiler that displays the section allocation in a GUI.
For details about the memory mapping profiler, see here.
 

Suitable Products
CS+ (formerly CubeSuite+)
  • 이 기사가 도움이 되셨나요?