메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

Confirmation of the effect of optimization (CS+)

Last Updated:05/17/2017

Question:

I am using the CS+ for CC Integrated Development Environment. Although I can specify “Optimization” in the compiler, is there any way to confirm the effect of optimization?

Answer:

Use the Optimization Performance Comparison Tool for the CS+ for CC Integrated Development Environment.
It automatically applies the build option for program optimization and allows you to compare and set how much the code size and execution speed are improved.

- By pressing a button, the code sizes and execution times for multiple build option patterns are shown.

-The measurements are color coded. You can easily identify a setting for the minimum code size and a setting for the fastest execution speed.

- The selected option pattern can be reflected to the project immediately.

To start the tool, select [Open the Optimization Performance Comparison Tool for active project...] from the [Build] menu in CS+ for CC.
This function is available in CS+ for CC V4.00.00 and later.

Click here for details of Optimization Performance Comparison Tool.

Suitable Products
CS+ (formerly CubeSuite+)
  • 이 기사가 도움이 되셨나요?