메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

Do I need to be careful in RAM parity error detection function of the MCU?

Latest Updated:04/24/2015

Question:

I am using the CC-RL compiler for RL78 devices. Do I need to pay particular attention to anything when using the RAM parity error detection function of the MCU?

Answer:

In the startup routine produced by creating a project in an IDE, initialization of the stack area is commented out. If you wish to use the RAM parity error detection function, enable the initialization of the stack area.
Suitable Products
e² studio
CS+ (formerly CubeSuite+)
C Compiler Package for RL78 Family