메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

Downloading manuals and sample programs (CS+)

Last Updated:05/17/2017

Question:

I am using the CS+ for CC Integrated Development Environment. Is it possible to download manuals or sample programs for the microcontroller selected for the project?

Answer:

Use the Smart Browser for the CS+ for CC Integrated Development Environment.

It allows you to display the latest documents about the microcontroller specified for the active project or download sample code provided with the application note without using a Web browser.

To start the Smart Browser, select [Smart Browser] in the [View] menu of CS+ for CC.

This function is available in CS+ for CC V4.01.00 and later.

Click here for details of the Smart Browser.

Suitable Products
CS+ (formerly CubeSuite+)
  • 이 기사가 도움이 되셨나요?