메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

E0203001 Message CS+

Last Updated:12/20/2017

Question:

I am using the CS+ integrated development environment.
After upgrading the version to CS+ in an environment with CubeSuite+, the following error occurred when building.

E0203001
An error occurred during build.
[Direct Error Cause]
The system cannot find the file specified.

How do I resolve this?
 

Answer:

The error occurred because the compiler version specified in the CubeSuite+ project does not exist in the CS+ installed environment. Try to resolve the error by the following procedure.(The following example is for RX Family.)

Right-click on [CC-RX (Build tool)] in the Project Tree panel, and then select [Properties]. In the version information category of the [Common Options] tabbed page, from the right pull-down menu, change the settings of [Using compiler package version]. From the right pull-down menu, specify the version to be used in [Using compiler package version].(Then, the installed version is displayed.)

For using the compiler which you were using with CubeSuite+ with CS+, refer to the following FAQ.
To use earlier version of compiler with CS+ V3.00.00 or later

Suitable Products
CS+ (formerly CubeSuite+)
  • 이 기사가 도움이 되셨나요?