메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

File Created during Startup of CS+

Last Updated:11/22/2017

Question:

What is the file that is created during startup of CS+ and automatically generated at next startup even if deleted?

Answer:

A file named "xxxx.mtud" is automatically created when CS+ starts.

Note: The "xxxx.mtud" file contains project configuration information such as the panel position and breakpoint position. If this file has been deleted, CS+ starts with the default setting and automatically creates a new file.

Suitable Products
CS+ (formerly CubeSuite+)
  • 이 기사가 도움이 되셨나요?