메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

How do I eliminate the error using CC-RL compiler for RL78 devices?

Latest Updated:07/14/2015

Question:

I am using the CC-RL compiler for RL78 devices. I get the error message below when I try to define an interrupt function. How do I eliminate this error?

E0520014: Extra text after expected end of preprocessing directive.

Answer:

A file iodefine.h is generated when you create a project in an IDE. Include iodefine.h before issuing the #pragma interrupt, since it has definitions for the names of interrupt requests.

You can designate inclusion of the file by a directive as shown above or by designating it with the compiler’s –preinclude option.

Example) -preinclude=iodefine.h

Suitable Products
e² studio
CS+ (formerly CubeSuite+)
C Compiler Package for RL78 Family
  • 이 기사가 도움이 되셨나요?