메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

How to change multiple build mode settings by one operation(CS+)

Last Updated:06/21/2017

Question:

I am using the CS+ for CC integrated development environment. I create multiple build modes in a project. I want to apply some setting to the multiple build modes by one operation. Is there any way to do that?

Answer:

In CS+ for CC V4.00.00 or later, the [Change property value for all build modes at once] item is provided in the [Build Mode] category in the [Common Options] tab of the build tool property.

You can set this item to [Yes] to apply the value set in the property to all build modes.
However, you need to be careful with enabling this item because the setting value might not be appropriate for other build modes.
For details about the common options of the build tool property, see the relevant Build Tool Operation manual for each family.

Suitable Products
CS+ (formerly CubeSuite+)
  • 이 기사가 도움이 되셨나요?