메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

How to erase error when assembly statements included in C-source file?

Latest Updated:11/21/2014

Question:

I am using the CA78K0R compiler for RL78 and 78K0R products. When I include assembly statements in a C-source file, I get the following warning message, an object file is not created, and an error occurs at the time of linkage. How do I eliminate this error?
W0837 Output assembler source file, not object file

Answer:

When a C-source file includes assembly statements, the compiler outputs warning message W0837, creates assembly source code, and ends processing.
The warning message W0837 indicates that an assembly source (*.ASM) file will be output instead of an object file (*.REL), even if the -o option has been set to specify the creation of an object-module file.
Therefore, since an object-module file for linking does not exist, building will fail.
When setting compiler options, specify the assembly-source file creation specification option, -SA or -A.
For CubeSuite+, specify a setting other than [No] for [Output assemble file] on the [Compile Options] tabbed page in the [Property] panel of the build tool.
Suitable Products
CS+ (formerly CubeSuite+)
C Compiler Package for RL78 and 78K Families
Compiler for RL78 Family and 78K0R [CA78K0R]
  • 이 기사가 도움이 되셨나요?