메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

Is RX C/C++ compiler license bought with CS+ valid for e² studio, too?

Latest Updated:09/04/2015

Question:

Is the RX C/C++ compiler license bought with CS+ valid for e² studio, too?

Answer:

RX C/C++ compilers having the major version number 2.X which are included in a CS+ (formerly called CubeSuite+) package can be integrated into e² studio using the current license.

For example, if the compiler supplied with CS+ (or CubeSuite+) was V2.00.01, then all V2.X RX C/C++ compiler versions (e.g. V2.01.00, V2.01.01, V2.02.00, ...) can be integrated into e² studio using the current valid licenses.

How to add toolchain:
To use CS+ or CubeSuite+ toolchain,

  1. Press toolbar button of "Integrate non-integrated toolchain" to open "Renesas Toolchain Management" view.
  2. Check desired toolchain(s).
    If desired product(s) were not listed, press [Add] button and specify the installed location.

    CS+ and CubeSuite+ toolchains are typically at the following location, described CCRX for example:
    CS+: C:/Program Files/Renesas Electronics/CS+/CC/CC-RX/(version number)
    CubeSuite+: C:/Program Files/Renesas Electronics/CubeSuite+/CC-RX/(version number)

 

Note:This FAQ is subjected to be applied to Asian area license distributions.

Suitable Products
e² studio
CS+ (formerly CubeSuite+)
C/C++ Compiler Package for RX Family