메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

Is there any way of installing CS+ V3.00.00 all at once?

Latest Updated:02/26/2015

Question:

Is there any way of installing CS+ V3.00.00 all at once?

Answer:

With the evaluation version, there is no way of installing the whole of CS+ V3.00.00 in a single sequence of operations.
CS+ V3.00.00 is divided into the two versions below. Install them individually.

  • CS+ for CC
  • CS+ for CA, CX

If you have purchased a compiler product, you can install CS+ V3.00.00 in a single sequence of operations by using the installer which the package of the compiler contains.

Suitable Products
CS+ (formerly CubeSuite+)