메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

Measurement of CAN Reception Time_CS+

Last Updated:10/18/2017

Question:

I am using the CS+ for CC integrated development environment. Can I measure the time from reception of a target CAN frame to processing of the CAN communication application?

Answer:

Use the E2 emulator and the function of measuring times for CAN bus reception of the CS+ for CC integrated development environment.

The function of measuring CAN bus reception processing times can improve problems with the speed performance of CAN communication applications. (RH850 only)

    You can easily measure the response time from frame reception to processing program start (important for CAN communications).
    You can stop the program when response time exceeds the specified value.
    After the program is stopped, you can check the trace data and CAN communication history.

This function is available in CS+ for CC V6.00.00 and later.
Details about measuring CAN bus reception processing times can be found on this page.

Also refer to the application notes.

    CAN Communication Time Measurement Solution (E2 Emulator, CS+)

Suitable Products
CS+ (formerly CubeSuite+)
E2 Emulator
  • 이 기사가 도움이 되셨나요?