메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

No header file for device’s SFR definitions in new project Cube Suite+

Latest Updated:04/12/2012

Question:

I created a new project with CubeSuite+ but I can’t find the header file for the device’s special function register (SFR) definitions and I can’t determine the SFR definitions.

Answer:

The SFRs are defined in a binary file called a device information file (DIF) on CubeSuite+ and the user cannot reference the actual definitions.

SFRs are defined using the Symbol as listed in the SFR List, located in the section titled “Special function registers (SFRs)”on User's Manual: Hardware.

Suitable Products
CS+ (formerly CubeSuite+)