메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

Relationship between variables and functions (CS+)

Last Updated:05/17/2017

Question:

I am using the CS+ for CC Integrated Development Environment. Is there any way to confirm which function accesses a variable?

Answer:

Use the Functions and Variables Access Table for the CS+ for CC Integrated Development Environment.

This table allows you to confirm the variables each function accesses (read or write).

To view the table, select [Functions and Variables Access Table] in the [View] menu of CS+ for CC.

This table is available in CS+ for CC V4.00.00 and later.

Suitable Products
CS+ (formerly CubeSuite+)
  • 이 기사가 도움이 되셨나요?