메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

Getting Started with e² studio

Last Updated:2/8/2017

Question:

Which manual should I to get started with e² studio?

Answer:

First, See the User's Manual Getting Started Guide.
It provides information on all the basic operations such as how to install e² studio, create a project, build, and debug. (For the build and debug configurations, see Help in the e2 studio GUI.)
It includes helpful information, classified by feature and device family.
If you can't find the information which you are looking for, use the search function in the Help menu. For the details of compiler and linker options, see the appropriate manual or Help for the compiler product.
 (You can find the manual for the compiler product in the installation folder of the compiler.)
 


Suitable Products

e² studio
  • 이 기사가 도움이 되셨나요?