메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

How to uninstall e² studio

Latest Updated:12/05/2016

Question:

Although I have installed multiple versions of e2 studio, Only one is listed in the "Program and Features" (or "Apps & Features") of the Windows Control Panel.
How do I uninstall the others which are not listed?

Answer:

e2 studio has uninstaller (ex: C:\Renesas\e2_studio\uninstall\uninstall.exe) in its installation folder. Executing the uninstall.exe, you will be able to uninstall the undesired e2 studio by visiting the folder.
Suitable Products
e² studio
  • 이 기사가 도움이 되셨나요?