메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

Pin Configurator is not displayed in e² studio

Last Updated:06/14/2017

Question:

Although Code Generator for RL78 is available in e² studio, Device Pin List and Device Top View are not available.

Answer:

When you use Code Generator in e² studio, in the following RL78 groups, Device Pin List and Device Top View are not available. Even though you start the tool, the list and view are displayed in blank.

・RL78/G12, RL78/G13, RL78/G14, RL78/G1A
・RL78/F12, RL78/F13, RL78/F14, RL78/F15
・RL78/L12, RL78/I1A

* The code generation function is available.

 The code generation function is available.

Device Pin List and Device Top View are not displayed.

Suitable Products
e² studio
Code Generator
  • 이 기사가 도움이 되셨나요?