메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

Why did I received an error while doing e2 studio integration on PDG?

Latest Updated:08/20/2015

Question:

"Please install Integration Service" error message has appeared while attempting to do "e2 studio integration" on PDG (Peripheral Driver Generator Version 2). "Integration Service" has already been installed.

Answer:

COM Objects have to be registered before using PDG2.

Please visit "e² studio Integration Service" page of e² studio Help, then please register COM Objects as the description.

Suitable Products
e² studio
  • 이 기사가 도움이 되셨나요?